U-Boot environment variables from MfgTool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot environment variables from MfgTool

Jump to solution
4,242 Views
kasperholtze
Contributor I

Hello,

Is it possible to set U-Boot environment variables using MfgTool? If so, how?

Thanks,

Kasper Holtze

Labels (1)
Tags (2)
1 Solution
2,775 Views
raymondwang
Senior Contributor I

You can create your env binary and download to flash via MFG tool.

FYI.

mkenvimage: a tool to generate a U-Boot environment binary image

View solution in original post

4 Replies
2,775 Views
LeonardoSandova
Specialist I

nice tool.

There are also U-boot scripts, quite useful to fetch and execute the same set of instructions in multiple boards. I have not touch this link for a long time, but you may start with this

Running a Script in U-boot

0 Kudos
Reply
2,776 Views
raymondwang
Senior Contributor I

You can create your env binary and download to flash via MFG tool.

FYI.

mkenvimage: a tool to generate a U-Boot environment binary image

2,775 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi raymond,

It's really helpful information from you ~~

Thanks.

Best Regards,

Dan

0 Kudos
Reply
2,775 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kasper,

It can not support setting U-Boot environment variables, but only can download u-boot, uImage and fs to flash. It's a download tool.

Best Regards

Dan