U-Boot commands for imx8m mini android environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot commands for imx8m mini android environment

1,138件の閲覧回数
Ruban1
Contributor II

U-Boot commands for imx8m mini android 11 environment

i tried according to the Documents

U-Boot > setenv bootargs
U-Boot > saveenv

U-Boot > setenv bootargs

U-Boot > boota

The process is not completing  its rebooting after 

[ 14.245666] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout:b
[ 14.262191] init: Failed to mount required partitions early ...
[ 14.269358] init: InitFatalReboot: signal 6
[ 14.277395] init: #00 pc 00000000000afe30 /system/bin/init
[ 14.283068] init: #01 pc 000000000004cd90 /system/bin/init
[ 14.288671] init: #02 pc 0000000000013ab0 /system/lib64/libbase.so
[ 14.295011] init: #03 pc 0000000000013090 /system/lib64/libbase.so
[ 14.301297] init: #04 pc 0000000000075b1c /system/bin/init
[ 14.306902] init: #05 pc 000000000002e0ec /system/bin/init
[ 14.312542] kvm: exiting hardware virtualization
[ 14.312875] imx-sdma 302b0000.dma-controller: external firmware not found, using ROM firmware
[ 14.312929] cfg80211: failed to load regulatory.db
[ 14.313004] imx-sdma 302c0000.dma-controller: external firmware not found, using ROM firmware
[ 14.313071] imx-sdma 30bd0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 14.313076] imx-sdma 30bd0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 19.269982] init: Reboot ending, jumping to kernel
[ 35.880671] VSD_3V3: disabling
[ 47.488649] random: crng init done

 

Do you have any other procedure for Android  11 in mincom U-BOOT commands

while running in minicom it display 4 Penguin and NXP .. it doesnot show Android symbol or proceed to Android OS

i have done everything according to the NXP document

Build is sucessful

Flashing to SD is sucessful

Kindly provide U-Boot commands for Android to get into Android OS

0 件の賞賛
返信
1 返信

1,128件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信