U-Boot Parallel LCD Support for iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot Parallel LCD Support for iMX6

1,970 Views
erezsteinberg
Contributor IV

Hello experts,

I'm trying to add support for parallel LCD in U-Boot for i.MX6DL.

Are there any guidelines how to do this?

(The latest U-Boot code seems to have LVDS and HDMI support, but I'm not sure about LCD).

Sincerely,

Erez

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,393 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erez

below links may be useful

wandboard: add Future Eletronics 7" WVGA LCD extension board · Freescale/u-boot-fslc@07425b2 · GitHu...

http://boundarydevices.com/displaying-a-splash-screen-with-u-boot/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply