U-Boot Parallel LCD Support for iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot Parallel LCD Support for iMX6

1,935件の閲覧回数
erezsteinberg
Contributor IV

Hello experts,

I'm trying to add support for parallel LCD in U-Boot for i.MX6DL.

Are there any guidelines how to do this?

(The latest U-Boot code seems to have LVDS and HDMI support, but I'm not sure about LCD).

Sincerely,

Erez

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,358件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erez

below links may be useful

wandboard: add Future Eletronics 7" WVGA LCD extension board · Freescale/u-boot-fslc@07425b2 · GitHu...

http://boundarydevices.com/displaying-a-splash-screen-with-u-boot/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信