U-Boot Nand identification problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot Nand identification problem

1,241 Views
LarsChristensen
Contributor I

I'm trying to move the U-Boot environment to NAND instead of MMC, but U-Boot doesnt seem to recognize the NAND chip.

I've succesfully used the mfg tools to write uboot to nand, and its booting off nand with no problems. Linux is also running smoothly of the nand (including rootfs).

When printing the id_bytes passed to nand_device_get_info in gpmi_nfc_mil.c, I get different results when its done by uboot vs linux.

Linux is giving me 0x2c, 0x48, 0x00, 0x,26, 0xa9, 0x00
uboot is printing out 0x2c, 0x2c, 0x2c, 0x2c, 0x2c, 0x2c and the nand is therefore not found in the list. Ive verified that the nand chip is in the list. But when forcing to use that chip (writing the correct values to the id_bytes) the result is a lot of DMA errors.

Any help solving this problem is greatly appreciated.

Thanks,
Lars

Labels (1)
0 Kudos
Reply
0 Replies