Two Separate MIPI-CSI Input Streams for Stereo Vision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two Separate MIPI-CSI Input Streams for Stereo Vision

Jump to solution
2,292 Views
kevin_keryk
Contributor I

Hello NXP Team,

I have a question for you about the i.MX 8M Plus ISP capability that I was not able to find an answer to by reading the i.MX 8M Plus documentation.

We have our stereo vision cameras already working with the NXP development board, but we want to plan accordingly for finalization of a camera adapter board for our own system.

When targeting our system, we will have access to a camera on a x4 MIPI CSI lane and another camera on a x2 MIPI CSI lane.  I wanted to verify whether the integrated ISP could support simultaneous input from two separate camera input streams for a stereo vision application.  Is this possible with the support in place for the ISP today?

Thanks,

-Kevin

0 Kudos
Reply
1 Solution
2,276 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, imx8mp can support dual camera via different ISP , you can refer to the basler dts file as reference, which supports two 4-lanes basler via dual ISP

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-d..."

 

View solution in original post

0 Kudos
Reply
1 Reply
2,277 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, imx8mp can support dual camera via different ISP , you can refer to the basler dts file as reference, which supports two 4-lanes basler via dual ISP

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-d..."

 

0 Kudos
Reply