TwinDie Single Rank LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TwinDie Single Rank LPDDR4

5,630件の閲覧回数
IvanCa
Contributor II

Hello Everyone

Does i.MX.8M.Mini support TwinDie LPDDR4?

TwinDie requires additional DG1 for addressing x8 and ZQ.

IvanCa_0-1605716936466.png 

IvanCa_1-1605716983154.png

Thanks

 

0 件の賞賛
返信
8 返答(返信)

5,558件の閲覧回数
twmemphis
Contributor III

To be exact it is not related to the number of dies. Modern LPDDR4 use 4 or sometimes even 8 dies per component! Important for you is just that you correctly wire the address, bank, bank group and chip-select lines.

The largest LPDDR4 device currently on the market as 64Gbit (=8 GB!) and comes from Micron: https://www.memorydistri.com/mt53e2g32d4dt-046%20wt:a.html

Other manufacturers like Samsung, Hynix, Nanya go to maximum 32Gbit with their LPDDR4 and only offer the big 64Gb size on LPDDR4X (with lower I/O voltage of 0.6V) only. As I understand the i.MX8 processors are not able to operate LPDDR4X, but only LPDDR4.

5,623件の閲覧回数
Yuri
NXP Employee
NXP Employee

@IvanCa 
Hello,

  Looks like You mean signals BG0/1 for DDR4. Use Table 16 (DDR3L/LPDDR4/DDR4 connectivity)
of Hardware Development Guide for the i.MX8Mm:

https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG

 

Regards,
Yuri.

0 件の賞賛
返信

5,618件の閲覧回数
IvanCa
Contributor II

Hello Yurii

Right, it is BG0/1, typo. But the question is still up. In case I use TwinDie DDR memory I can use only one memory controller of iMX8MINI (MIMX8MM5DVTLZAA). To use two TwinDie chips/controllers I need two extra bits of the Bank Group (BG) signals to address other memory groups on the second memory chip?

Thanks, Ivan

0 件の賞賛
返信

5,579件の閲覧回数
Yuri
NXP Employee
NXP Employee

@IvanCa 
Hello,

   Customers can use i.MX8Mn DDR4 design as an example.

https://www.nxp.com/downloads/en/schematics/8MNANOD4-EVK-DF-SCH.7z

 

Regards,
Yuri.

0 件の賞賛
返信

5,575件の閲覧回数
IvanCa
Contributor II

Hello Yurii.

Reference design schematic, you guess I can add one more DDR4 device since BG0 and BG1 are engaged?

Thanks

 

0 件の賞賛
返信

5,566件の閲覧回数
Yuri
NXP Employee
NXP Employee

@IvanCa 
Hello,

   Yes - use  one more DDR4.

Regards,
Yuri.

0 件の賞賛
返信

5,573件の閲覧回数
IvanCa
Contributor II

It seems I got the idea already.

Thanks Yurii

5,609件の閲覧回数
Yuri
NXP Employee
NXP Employee

@IvanCa
Hello,

   Basically connection scheme for DDR4 is shown in the  Table 16 (DDR3L/LPDDR4/DDR4
connectivity). Signals BG0 and BG1 are shown there.
  But we  have not tested an example for the case with BG1 using.

Regards,
Yuri.

0 件の賞賛
返信