Tutorials on Setting Up device tree in Yocto for routing GPIO to Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tutorials on Setting Up device tree in Yocto for routing GPIO to Pins

2,999 Views
mitchponv
Contributor I

Good afternoon,

I have been looking everywhere and I cannot find a tutorial or any instructions on how to configure the Yocto kernel to mux any of the GPIOs in Linux to physical pins on Imx6.

This should be a very basic entry level introduction on how to work with the Yocto SDK, and should provide step by step instructions

I currently have a Yocto installation from this tutorial: Yocto Project Quick Start

And an Imx6 Hummingboard

If someone can please help such tutorial, I would greatly appreciate it.

Thank you,

Tags (2)
0 Kudos
Reply
1 Reply

2,208 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dmitry

I am not aware of such tutorial, in general one can look at:

http://www.kosagi.com/w/index.php?title=Definitive_GPIO_guide

http://xillybus.com/tutorials/device-tree-zynq-1

http://devicetree.org/Device_Tree_Usage

linux folder Documentation/devicetree/bindings/pinctrl/fsl,imx6q-pinctrl.txt

Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply