Trying to run GeexBox on iMx6 . Getting problem while mounting root file system.....

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trying to run GeexBox on iMx6 . Getting problem while mounting root file system.....

8,391件の閲覧回数
brajeshsharma
Contributor II

Hello Members ,

I am trying to get Geexbox onto iMx6 , for that i am using Openbricks sdk which have given me the kernel image and rootfile system . Before trying the iMx6 with rootfs of openbricks i have tested it with the rootfs provided by freescale and the sabresd board is able to comfortably booting , loading kernel and mounting rootfs . But when i try the same thing with rootfs i got from Openbricks it got stuck right after the following line .

---------------------------------------------------------------

"VFS: Mounted root (nfs filesystem) on device 0:12.

Freeing init memory: 168K"

-----------------------------------------------------------------

It doesnt respond after these lines . How do i fix it and get the prompt as i am getting with freescale rootfs ?

Thanks & Regards

Brajesh Sharma

ラベル(2)
0 件の賞賛
返信
15 返答(返信)

7,960件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Brajesh,

The problem of "VFS: Mounted root (nfs filesystem) on device 0:12" is caused by network. You should restart the nfs service:

sudo /etc/init.d/nfs-kernel-server restart

Hope this can help you~~

Best Regards

Dan

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi Dan ,

Thanks a lot for replying to my query . As you suggested i'v restarted the

nfs-server few times but still it is stuck at that point though there is no

such problem when i try with rootfs provided by freescale .

Do you have an idea what might be the problem here ?

Thanks & Regards

Brajesh Sharma

0 件の賞賛
返信

7,960件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Brajesh,

Which board are you using?

Best Regards

Dan

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi Dan ,

I am using SabreSD (iMX6) board

Regards

Brajesh

0 件の賞賛
返信

7,960件の閲覧回数
LeonardoSandova
Specialist I

Brajesh, post the whole kernel log.

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

hi ,

I was trying the same thing with root file system of geexbox for Cubox on

sabreSD since both have same imx6q but exactly same output came and stuck

at

"VFS: Mounted root (nfs filesystem) on device 0:12.

Freeing init memory: 168K"

if you have any idea about this please share !

Thanks& regards

Brajesh

0 件の賞賛
返信

7,960件の閲覧回数
LeonardoSandova
Specialist I

Can you mount the same filesystem (FS) on your Linux host machine? can you boot and use the FS on a SD card?

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi ,

Thanks for replying . I'v seen few user guides on how to setup SD card for

imx but all that is a bit complicated that using a NFS Server but i'll try

as you'r saying that may help . And i did'nt get you "Can you mount the

same filesystem (FS) on your Linux host machine?" . I have mounted FS on

linux machine from there i am using it as Network file system . Are you

asking me to do something else ?

I'll update soon after trying setting up the SD Card .

Thanks & Regards

Brajesh Sharma

On Tue, Nov 19, 2013 at 8:46 AM, Leonardo Sandoval Gonzalez <

0 件の賞賛
返信

7,960件の閲覧回数
LeonardoSandova
Specialist I

Correct, you did the test I asked. Let us know the results of the SD case. How are you exporting your folder (post the /etc/exports file)?

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi ,

As you asked i have tried to set up SD card also but no response from

Sabre. So after that i just loaded the card with u-boot image only by dd

command , but when i insert it in board no response at all though i am sure

boot switch mode is right since other card with u-boot is giving the u-boot

prompt but i dont have any idea how that card was partitioned or set-up .

Need suggestion on it from you since i am stuck in here since long time .

Regards & Thanks

Brajesh

0 件の賞賛
返信

7,960件の閲覧回数
YixingKong
Senior Contributor IV

Brajesh

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

7,960件の閲覧回数
YixingKong
Senior Contributor IV

Brajesh

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel

free to reply with an update to this discussion.

Thanks,
Yixing

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi ,

I am trying to set up the SD card for android boo up as given on a

freeacale page :

https://community.freescale.com/docs/DOC-1232#jive_content_id_Additional_Resources

I have formatted and partitioned the card and loaded the images as

instructed there but still i cant get the even the bootloader . Although

there are few steps that i am confused with in the procedure . There is

no specific partition for u-boot and uImage i am copying them by dd command

in /dev/sdb by offset address and there are few more things in that page i

am having trouble with . I am trying to do this by my way or any other way

i find it on web , i'll update the results about it .

Thanks & Regards

Brajesh Sharma

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi ,

For NFS my /etc/exports content is :

0 件の賞賛
返信

7,960件の閲覧回数
brajeshsharma
Contributor II

Hi ,

Here is the boot arguments i have followed

0 件の賞賛
返信