Trying to build SCU FW binary using SCU porting kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trying to build SCU FW binary using SCU porting kit

3,539 Views
Ramprakash
Contributor II

Hi All,

I am trying to create a SCU FW binary by using the SCU Porting Kit. I have followed all the steps mentioned in the following link:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

But when i try to build the file SCU by using the command 

"make qx R=b0 B=myboard" i get the following error:

/bin/bash: /gcc-arm-none-eabi-*/bin/arm-none-eabi-gcc: No such file or directory
/bin/bash: /gcc-arm-none-eabi-*/bin/arm-none-eabi-gcc: No such file or directory
/bin/bash: /gcc-arm-none-eabi-*/bin/arm-none-eabi-gcc: No such file or directory
Generating platform/board/mx8qx_myboard/dcd/imx8qx_dcd_1.2GHz.h
/bin/bash: /gcc-arm-none-eabi-*/bin/arm-none-eabi-cpp: No such file or directory
Makefile:465: recipe for target 'platform/board/mx8qx_myboard/dcd/imx8qx_dcd_1.2GHz.h' failed
make: *** [platform/board/mx8qx_myboard/dcd/imx8qx_dcd_1.2GHz.h] Error 127

I have set path in the bashrc file

export TOOLS=/home/nikola/workspace/TCU_NXP/arm-gnu-embedded_toolchain

what am I missing here? I am building the SCU in ubuntu 16.4 system for i.MX8QX board.

Thanks and Regards,

Ramprakash

 

0 Kudos
Reply
4 Replies

3,525 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which version of the porting kit are you using?

0 Kudos
Reply

3,472 Views
Ramprakash
Contributor II

Hi @jimmychan ,

I am trying to use SCU v1.3 and my linux version is 4.14.98.

Thanks and Regards,

Ramprakash

0 Kudos
Reply

3,452 Views
jimmychan
NXP TechSupport
NXP TechSupport

Hello,

 

According to the Makefile, the CROSS_COMPILE is:

CROSS_COMPILE = $(TOOLS)/gcc-arm-none-eabi-*/bin/arm-none-eabi-

 

So, please check the PATH of the "TOOLS" that you export is correct.

0 Kudos
Reply

3,442 Views
Ramprakash
Contributor II

Hi @jimmychan ,

I did set the environment variable TOOLS in bashrc file and I am able to access the same from the command line by using the command "echo $TOOLS" but the same is not reflected when I try to run the make file. 

I did a workaround where I hardcoded the TOOLS variable in the makefile with the path and it worked. Do you have any idea why the TOOLS is not recognized when running the make file without hardcoding it.

 

Thanks and Regards,

Ramprakash

0 Kudos
Reply