Trouble setting up NFS for i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble setting up NFS for i.MX53

4,241件の閲覧回数
DatNguy
Contributor I

Hello,

I'm been trying to setup the i.MX53 to boot via NFS but having some problem.  Here is what I did and maybe someone can point out what I did wrong and how to fix it.  I'm pretty new with this so any help is greatly appreciated. I used the Adeneo 4.1 prebuilt files to build this setup.

Here is my IP info, using an Apple Ethernet Adapter

eth1 Link encap:Ethernet HWaddr 28:37:37:03:c5:f1

inet addr:192.168.1.2 Bcast:192.168.1.255 Mask:255.255.255.0

inet6 addr: fe80::2a37:37ff:fe03:c5f1/64 Scope:Link

UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1

RX packets:6585 errors:0 dropped:0 overruns:0 frame:0

TX packets:6581 errors:0 dropped:0 overruns:0 carrier:0

collisions:0 txqueuelen:1000

RX bytes:889944 (889.9 KB) TX bytes:7613344 (7.6 MB)


/etc/exports file

/home/daknguy/imx-android/nfsroot *(rw,no_root_squash,sync,no_subtree_check,insecure)

/home/daknguy/imx-android/tftproot *(rw,no_root_squash,sync,no_subtree_check,insecure)


daknguy@daknguy-System-Product-Name:/$ sudo mount -t nfs 192.168.1.2:/home/daknguy/imx-android/nfsroot /nfsroot

daknguy@daknguy-System-Product-Name:/$ cd /nfsroot/

daknguy@daknguy-System-Product-Name:/nfsroot$ ls

boot init proc sys u-boot.bin uImage

data init.freescale.rc ramdisk.img system ueventd.freescale.rc uramdisk.img

default.prop init.goldfish.rc recovery.img system.img ueventd.goldfish.rc

dev init.rc sbin system_inflexion.img ueventd.rc


MX53-LOCO U-Boot > printenv

bootdelay=3

baudrate=115200

loadaddr=0x70800000

netdev=eth0

ethprime=FEC0

bootdelay=3

uboot=u-boot.bin

kernel=uImage

loadaddr=0x70800000

rd_loadaddr=0x70D00000

vga=setenv bootargs ${bootargs} di1_primary video=mxcdi1fb:GBR24,VGA-XGA vga

lcd=setenv bootargs ${bootargs} di0_primary calibration

hdmi_720p=setenv bootargs ${bootargs} di0_primary video=mxcdi0fb:RGB24,1280x720M@60 hdmi gpu_nommu gpu_memory=64M

hdmi_1080p=setenv bootargs ${bootargs} di0_primary video=mxcdi0fb:RGB24,1080P60 hdmi gpu_nommu gpu_memory=64M

claa_lcd=setenv bootargs ${bootargs} di0_primary video=mxcdi0fb:RGB565,CLAA-WVGA calibration

bootargs_android=setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0

bootcmd_SD=run bootcmd_SD1 bootcmd_SD2

bootcmd_SD1=run bootargs_base set_display bootargs_android

bootcmd_SD2=mmc read 0 ${loadaddr} 0x800 0x2000;mmc read 0 ${rd_loadaddr} 0x3000 0x300;bootm ${loadaddr} ${rd_loadaddr}

bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm

bootcmd_android_recovery=run bootargs_base bootargs_android_recovery;mmc read 0 ${loadaddr} 0x800 0x2000;bootm

bootargs_android_recovery=setenv bootargs ${bootargs} init=/init root=/dev/mmcblk0p4 rootfs=ext4

ethact=FEC0

serverip=192.168.1.2

ipaddr=192.168.1.50

lvds=setenv bootargs ${bootargs} video=mxcdi0fb:RGB666,XGA ldb=di0 di0_primary

bootargs_base=set bootargs console =ttymxc0, 115200 ${lvds}

set_display=run lvds

bootcmd_nfs=run bootargs_base bootargs_nfs ; nfs ${loadaddr} ${serverip}:${nfsroot}/uImage;bootm

bootcmd=run bootcmd_nfs

bootargs=console =ttymxc0, 115200 setenv bootargs ${bootargs} video=mxcdi0fb:RGB666,XGA ldb=di0 di0_primary root=/dev/nfs ip=dhcp nfsroot=192.168.1.2:/nfsroot,v3,tcp

stdin=serial

stdout=serial

stderr=serial

nfsroot=/nfsroot



Environment size: 1862/131068 bytes

MX53-LOCO U-Boot > boot

FEC: enable RMII gasket

PHY indentify @ 0x0 = 0x0007c0f1

Using FEC0 device

File transfer via NFS from server 192.168.1.2; our IP address is 192.168.1.50

Filename '/nfsroot/uImage'.

Load address: 0x70800000

Loading: FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

*** ERROR: Cannot mount


If I change nfsroot to /home/daknguy/imx-android/nsfroot I get the following error “*** ERROR: Cannot umount

Environment size: 1887/131068 bytes

MX53-LOCO U-Boot > boot

FEC: enable RMII gasket

PHY indentify @ 0x0 = 0x0007c0f1

Using FEC0 device

File transfer via NFS from server 192.168.1.2; our IP address is 192.168.1.50

Filename '/home/daknguy/imx-android/nfsroot/uImage'.

Load address: 0x70800000

Loading: FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

FEC: Link is down 7809

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################*** ERROR: Cannot umount

## Booting kernel from Legacy Image at 70800000 ...

Image Name: Linux-2.6.35.3-01162-gecaa8dd-di

Image Type: ARM Linux Kernel Image (uncompressed)

Data Size: 3325320 Bytes = 3.2 MB

Load Address: 70008000

Entry Point: 70008000

Verifying Checksum ... OK

Loading Kernel Image ... OK

OK

Starting kernel ...

Initializing cgroup subsys cpu

Linux version 2.6.35.3-01162-gecaa8dd-dirty (rlorriaux@rl-linux) (gcc version 4.4.3 (GCC) ) #1 PREEMPT Mon Nov 14 15:00:29 PST 2011

CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f

CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

Machine: Freescale MX53 LOCO Board

Memory policy: ECC disabled, Data cache writeback

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 234496

Kernel command line: console =ttymxc0, 115200 setenv bootargs ${bootargs} video=mxcdi0fb:RGB666,XGA ldb=di0 di0_primary root=/dev/nfs ip=dhcp nfsroot=192.168.1.2:/home/daknguy/imx-anp

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

allocated 7864320 bytes of page_cgroup

please try 'cgroup_disable=memory' option if you don't want memory cgroups

Memory: 416MB 512MB = 928MB total

Memory: 924384k/924384k available, 25888k reserved, 0K highmem

Virtual kernel memory layout:

vector : 0xffff0000 - 0xffff1000 ( 4 kB)

fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

DMA : 0xf9e00000 - 0xffe00000 ( 96 MB)

vmalloc : 0xe0800000 - 0xf4000000 ( 312 MB)

lowmem : 0x80000000 - 0xe0000000 (1536 MB)

pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)

modules : 0x7f000000 - 0x7fe00000 ( 14 MB)

.init : 0x80008000 - 0x80039000 ( 196 kB)

.text : 0x80039000 - 0x80892000 (8548 kB)

.data : 0x808b2000 - 0x8091b6c0 ( 422 kB)

SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Hierarchical RCU implementation.

RCU-based detection of stalled CPUs is disabled.

Verbose stalled-CPUs detection is disabled.

NR_IRQS:368

MXC GPIO hardware

MXC IRQ initialized

MXC_Early serial console at MMIO 0x53fbc000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

console [tty0] enabled, bootconsole disabled






タグ(1)
0 件の賞賛
返信
7 返答(返信)

2,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

If you have prebuilt images, maybe you have the prebuild image for NFS folder.

the prebuild NFS folder will hold uramdisk and system.

Are you able to take uImage from network?

0 件の賞賛
返信

2,508件の閲覧回数
SyedRafiulHussa
Contributor II

Hi,

I need help regarding mounting android file system using NFS. I tried, however, it didn't work. 

I am using prebuilt image of uramdisk.img, system.img, and recovery.img. How can I build root file system using these images? 

Thanks in advance.

Syed Rafiul Hussain

0 件の賞賛
返信

2,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee
0 件の賞賛
返信

2,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Does your board ping your PC?

0 件の賞賛
返信

2,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

To make sure your file systems and NFS server is OK, please mount it somewhere on your PC:

sudo mount 192.168.1.2://home/daknguy/imx-android/nsfroot /mnt


Can you see all needed files? Is there any permission error?


If you can mount it, PC side is OK.



0 件の賞賛
返信

2,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

it´s not about rootfs.

He can not even take uImage.

Miroslav Tisma said:

I think that you have a wrong root filesystem. You have to extract the rootfs.tar.gz (you can build it by yourself, for example, buildroot filesystem) as a root user to /nfsroot.

0 件の賞賛
返信

2,508件の閲覧回数
MiroslavIMX53QS
Contributor I

I think that you have a wrong root filesystem. You have to extract the rootfs.tar.gz (you can build it by yourself, for example, buildroot filesystem) as a root user to /nfsroot.

0 件の賞賛
返信