Treck TCP/IP in NXP Linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Treck TCP/IP in NXP Linux BSP

Jump to solution
3,659 Views
zc_tee
Contributor III

Dear all,

May i know is Treck TCP/IP used in NXP provided BSP? We are using the linux BSPs for i.mx6 from NXP, and we are wondering if our devices is affected by the recent Ripple20 Vulnerabilities that happened in the Treck TCP/IP stack protocl.

Please advise. Thank you.

Labels (5)
0 Kudos
Reply
1 Solution
3,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZC Tee

I am afraid Treck is not supported, supported features are described in NXP

official linux documentation on

Embedded Linux for i.MX Applications Processors | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,527 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZC Tee

I am afraid Treck is not supported, supported features are described in NXP

official linux documentation on

Embedded Linux for i.MX Applications Processors | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,526 Views
zc_tee
Contributor III

Hi Igor,

Thanks for the fast respond.

May i know which document in particular that describes the supported features? I do not see it in the Linux Release Note, Linux User Guide or Linux Reference Manual.

Thank you.

Regards,

Tee

0 Kudos
Reply
3,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tee

 

from i.MX Linux Release Notes

pastedImage_1.jpg

 

Best regards
igor

0 Kudos
Reply
3,526 Views
zc_tee
Contributor III

Hi Igor,

Thank you. I got it now.

0 Kudos
Reply