Transition to RUN from STOP for A7 core (Linux).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transition to RUN from STOP for A7 core (Linux).

1,263 Views
JuanBrea
Contributor II

We are investigating methods for fastest transition to RUN from STOP for A7 core (Linux).    

  1. If an external 24MHz clock is used instead of the XTAL, will it speed up our wake time by avoiding the requirement for xtal lock  (XTALOSC_CTRL_24 register has bits for CLKGATE_DELAY and XTALOSC_PWRUP_DELAY—could we use the fastest selections)?
  2. If we instead leave the 24MHz xtal running, what would be the expected power impact? 
0 Kudos
Reply
1 Reply

1,214 Views
JuanBrea
Contributor II

Device is iMX7S

0 Kudos
Reply