Transient response Measures

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Transient response Measures

1,227件の閲覧回数
ban45
Contributor III
Transient response occurs during boot and DDR3 operation.

Operation method for lowering transient response,

If you have the know-how of register setting, wouldn't it just teach you?

The following measures are taken.

The pattern is thicker.
The capacitor is increasing.

0 件の賞賛
返信
1 返信

1,197件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori

>method for lowering transient response,

>If you have the know-how of register setting, wouldn't it just teach you

transients may be caused by strong signal, one can try to decrease drive

strength using DSE field in IOMUX pad register, described in AN5078

Influence of Pin Setting on System Function and Performance

For example for i.MX6Q sect.36.4.350 Pad Control Register
(IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK0_P)

i.MX 6Dual/6Quad Applications Processor Reference Manual

Also it may be caused by signal reflections, one can pay attention

to board layout, please check i.MX 6 Series Layout Recommendations

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信