Transfer stoped in fastboot downloading.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transfer stoped in fastboot downloading.

2,761 Views
alex_li
Contributor II

Hello!

   I download uboot from git://git.freescale.com/imx/uboot-imx.git accroding to document "Android user's guide"(rev:M6.0.1_2.1.0),and porting it accroding to "BSP porting guide" based on sabresd.

   Now i have a problem: transfer stop in fastboot mode.

log as below:

U-Boot 2015.04-dirty (Sep 18 2018 - 16:34:40)
CPU: Freescale i.MX6QP rev1.0 at 792 MHz

CPU: Temperature 37 C
Reset cause: WDOG
Board: MX6QP

I2C:ready
DRAM: 2 GiB

MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

Fastboot: Normal
flash target is MMC:1
Normal Boot
Hit any key to stop autoboot: 1 

=> fastboot
ptn 0 name='mbr' start=0 len=1
ptn 1 name='bootloader_nor' start=1024 len=524288
ptn 2 name='kernel_nor' start=524288 len=7536640
ptn 3 name='recovery_nor' start=8060928 len=65536
ptn 4 name='burn_nor' start=0 len=8388608
ptn 5 name='boot' start=2048 len=20480
ptn 6 name='sdcard' start=40960 len=20480
ptn 7 name='system' start=63488 len=5242880
ptn 8 name='recovery' start=5306368 len=40960
ptn 9 name='data' start=5349376 len=11468800
ptn 10 name='cache' start=16820224 len=262144
ptn 11 name='private' start=17084416 len=1048576
ptn 12 name='resc' start=18135040 len=1048576
ptn 13 name='bootb' start=19185664 len=40960
ptn 14 name='recoveryb' start=19228672 len=40960
ptn 15 name='systemb' start=19271680 len=5242880
ptn 16 name='map' start=24516608 len=36450304
Starting download of 1293389240 bytes
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
..........................................................................
....................................

no error report,not exit ,just stop transfer data. No error report in PC.

Anybody can help me?

Thanks!

Labels (2)
0 Kudos
Reply
4 Replies

2,553 Views
alex_li
Contributor II

My mistake!

We use EIM_D22 pin as ECSPI4_MISO in our board,which is not fit the sabresd board. So I mask USB code, which cause this problem.

Error port:

static iomux_v3_cfg_t const usb_otg_pads[] = {
/* Disable usb power control
*/
// MX6_PAD_EIM_D22__USB_OTG_PWR | MUX_PAD_CTRL(NO_PAD_CTRL),
// MX6_PAD_ENET_RX_ER__USB_OTG_ID | MUX_PAD_CTRL(OTG_ID_PAD_CTRL),
};

static iomux_v3_cfg_t const usb_hc1_pads[] = {
/* Disable usb power control
*/
// MX6_PAD_ENET_TXD1__GPIO1_IO29 | MUX_PAD_CTRL(NO_PAD_CTRL),
};

static void setup_usb(void)
{
/* Disable usb power control
*/
// imx_iomux_v3_setup_multiple_pads(usb_otg_pads,
// ARRAY_SIZE(usb_otg_pads));
//
// /*
// * set daisy chain for otg_pin_id on 6q.
// * for 6dl, this bit is reserved
// */
// imx_iomux_set_gpr_register(1, 13, 1, 0);
//
// imx_iomux_v3_setup_multiple_pads(usb_hc1_pads,
// ARRAY_SIZE(usb_hc1_pads));
}

Correct port:

static iomux_v3_cfg_t const usb_otg_pads[] = {
/* Disable usb power control
*/
// MX6_PAD_EIM_D22__USB_OTG_PWR | MUX_PAD_CTRL(NO_PAD_CTRL),
MX6_PAD_ENET_RX_ER__USB_OTG_ID | MUX_PAD_CTRL(OTG_ID_PAD_CTRL),
};

static iomux_v3_cfg_t const usb_hc1_pads[] = {
MX6_PAD_ENET_TXD1__GPIO1_IO29 | MUX_PAD_CTRL(NO_PAD_CTRL),
};

static void setup_usb(void)
{
imx_iomux_v3_setup_multiple_pads(usb_otg_pads,
ARRAY_SIZE(usb_otg_pads));

/*
* set daisy chain for otg_pin_id on 6q.
* for 6dl, this bit is reserved
*/
imx_iomux_set_gpr_register(1, 13, 1, 0);

imx_iomux_v3_setup_multiple_pads(usb_hc1_pads,
ARRAY_SIZE(usb_hc1_pads));
}

0 Kudos
Reply

2,553 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi min,

Its difficult to see which is the error, So please check:

https://community.nxp.com/thread/448862 

Regards

0 Kudos
Reply

2,553 Views
alex_li
Contributor II

@Bio_TICFSL

We fix this problem, and post resolution.Thanks for your help.

BR!

0 Kudos
Reply

2,553 Views
alex_li
Contributor II

Dear Bio:

         I have problem in fastboot,not fast boot.

        Any advice?

BR!

0 Kudos
Reply