Touch input not working in IMX RT 1050 FT 5336 IC using emwin library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Touch input not working in IMX RT 1050 FT 5336 IC using emwin library

1,116件の閲覧回数
yvkrkrishna
Contributor III

Hi i am using IMX RT 1050 EVK Board with LCD 480x272. I have made custom GUI and flashed to the board. Touch input is working properly.

But when i am flashing to custom board with LCD Display size 800x472. I am able to flash the custom made GUI in app wizard software to the board.

Problem is:

Touch input is working only in first quadrant of LCD Display.

Could any one please tell me what configuration to be updated for LCD size 800x272 with FT 5336 Touch IC.

 

Regards

Krishna Reddy

0 件の賞賛
返信
1 返信

1,102件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could anyone please tell me what configuration to be updated for LCD size 800x272 with FT 5336 Touch IC?
-- I think I need more information.
Firstly, I'd like to know whether LCD (800x472) works with the IMX RT 1050 EVK, then I was wondering if you can introduce the testing GUI demo briefly.
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信