Touch control?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Touch control?

1,575 次查看
HaiDangSon
Contributor I

Hi every one.

I have some trouble about the touch lcd.

The freescale's lcd is seiko 43WVFIG. That's work good.

My lcd is ampire AM-800480L with the same resolution but the size is bigger, that's display well.

Both of them have the touch panel with 4 line connect to imx53.

I use the seiko driver to control ampire.I can touch the panel of ampire but the imx not get right position ( error about 2-3mm, I just measure by my eye).

I don't familliar with os system, that's I can't understand how it works.

My question is:

- I want to debug the position when I touch to the panel of LCD.

What file I need to modify to printf the x-y position to visual 2008 (in debug mode)?

After that I want to modify to make imx53 understand right position.

- If possible, can you explain what OS system work? Does it like the microcontroller work in file main.c and if interrupt happen that jump to interrupt function?

Thanks in advance.

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数