Totem player does not release resource when exits.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Totem player does not release resource when exits.

1,430件の閲覧回数
franklee19731
Contributor I

Totem player on Ubuntu does not release all the resource when it exits.

When I start totem on a terminal to play an mp4 file, it prints it uses "aiur", "vpudec",  and "mfw_v4lsink", after I close totem, it only print "[--->FINALIZE aiurdemux", I have no idea if it release vpudec and mfw_v4lsink.

I do not know if this problem will me a substantial issue for the use of totem.

ラベル(4)
0 件の賞賛
返信
1 返信

1,308件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

hmm, i have never noticed that, but I haven't seen problems whenever I use totem, so I guess it does releases them.

Let me check if I can verify that, but as I see, there is no problem when using Totem

0 件の賞賛
返信