Totem player does not release resource when exits.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Totem player does not release resource when exits.

1,030 Views
franklee19731
Contributor I

Totem player on Ubuntu does not release all the resource when it exits.

When I start totem on a terminal to play an mp4 file, it prints it uses "aiur", "vpudec",  and "mfw_v4lsink", after I close totem, it only print "[--->FINALIZE aiurdemux", I have no idea if it release vpudec and mfw_v4lsink.

I do not know if this problem will me a substantial issue for the use of totem.

Labels (4)
0 Kudos
Reply
1 Reply

908 Views
SergioSolis
NXP Employee
NXP Employee

hmm, i have never noticed that, but I haven't seen problems whenever I use totem, so I guess it does releases them.

Let me check if I can verify that, but as I see, there is no problem when using Totem

0 Kudos
Reply