Toshiba Toggle Flash inquiry

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Toshiba Toggle Flash inquiry

1,966 Views
shai_b
Senior Contributor II

Dear Team,

 

My customer has a small question about using NAND regarding the USB1_SS_SEL pin.

Can you please advise how to connect the USB1_SS_SEL pin when using Nand Flash?

imx8mnand.png

Waiting for your kind feedback, many thanks.

Best Regards,

Shai

Labels (1)
4 Replies

1,950 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @shai_b,

I hope you are doing well.

Are you looking to use NAND_RE functionality and USB1_SS_SEL functionality as well?

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

1,946 Views
shai_b
Senior Contributor II

@riteshmpatel Helllo,

Yes, He wants to use the nRE functionality and USB1_SS_SEL functionality.

Thanks in advance 

KR,

Shai

0 Kudos
Reply

1,942 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @shai_b,

Thank you for the clarification.

USB1_SS_SEL is used as a GPIO. So, if one wants to use NAND_RE functionality, then USB1_SS_SEL shall be mixed with any other available GPIO.

Thanks & Regards,
Ritesh M Patel

1,935 Views
shai_b
Senior Contributor II

@riteshmpatel ,

 

Thanks a lot for your input.

Kind regards 

Shai

0 Kudos
Reply