Tool to compile IM6 source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tool to compile IM6 source code

2,427件の閲覧回数
lyfsci
Contributor III

Hi Experts,


Is there any installation or tool required to compile the linux source code of the IMX6 SL processor. for EVK ?

I had downloaded the IMX6 source code and was looking for tool to compile it.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,335件の閲覧回数
lyfsci
Contributor III

Thats great info.

0 件の賞賛
返信

2,335件の閲覧回数
Yuri
NXP Employee
NXP Employee

   It may be recommended to use the recent Linux BSP(s) for i.MX6 (SL ).

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.2_iMX6SL_BUNDLE&appType=license&locat...

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_IMX6SL_BUNDLE&appType=license&locat...

http://cache.freescale.com/files/32bit/doc/support_info/IMX6YOCTOPATCHRN.pdf

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&appType=license&location...

The documentation package (L3.10.17_1.0.0_LINUX_DOCS) / file (IMX6YOCTOPATCHRN.pdf)

contains information how to setup host environment and build target system.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信