Toaster Quick Start Guide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Toaster Quick Start Guide

4,706件の閲覧回数
vardhmanmodi
Contributor II

Hello,

I want to use Toaster for building the NXP's yocto release 4.1.15_2.0.0. While exploring the community. I came across the "HOB quick start guide" available at https://community.nxp.com/docs/DOC-102505.

Is there a similar "Toaster quick start guide" for building NXP's yocto release using Toaster?

ラベル(3)
タグ(2)
4 返答(返信)

4,244件の閲覧回数
andreyreyes
Contributor II

Vardhmal - Did you made any progress? I'm trying to get this to work but I can't get Toaster to see the fls downloads.

A search in the community returns this but it seems like they stopped the effort.

https://community.nxp.com/message/388996 

Andrey

0 件の賞賛
返信

4,244件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vardhman

please check

http://www.yoctoproject.org/bulk/devday-eu-2014/ypdd14-reyna-toaster.pdf 

Toaster User Manual 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,244件の閲覧回数
andreyreyes
Contributor II

Igor - the referenced Toaster manual version is old (Revision 1.8 2015) and does not correspond to the 4.1.15_2.0.0 release which uses Krogroth. The presentation is from 2014-10-17 and a lot has changed since then.

Do you know which version of Krogroth was released with 4.1.15_2.0.0? Release date for 4.1.15_2.0.0 says 2017-01-18 which makes me think that it might be Krogroth 2.1.1 (2016-08) or 2.1.2 (2016-12), but from page 2, 2nd paragraph to last of the "i.MX Yocto Project User's Guide" document it says:

"Release L4.1.15_2.0.0_ga is released for Yocto Project 2.1 (Krogoth). The same recipes for Yocto Project 2.1 are going to be
upstreamed and made available on the next release of the Yocto Project release. The Yocto Project release cycle lasts roughly
six months."

That would be Revision 2.1 from 2016-04, is that correct?

0 件の賞賛
返信

4,244件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrey

please post this to meta-fsl-arm mailing list :
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor

0 件の賞賛
返信