To use the Debug output UART port as an Applications UART Port,

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To use the Debug output UART port as an Applications UART Port,

1,201件の閲覧回数
admin
Specialist II

Hi,


I want to disable the debug output of UART port & make use of it as my Applications UART Port.

I'm using IMX535 QSB with Android 2.3.3

Hope it is done at the time of booting but am not sure about the steps

Could you please tel me the steps of how to disable the debug output of UART port & make use it as Applications UART Port.

Kindly do the needful as soon as possible,

Many Thanks,

Srinivasan S

タグ(1)
0 件の賞賛
返信
1 返信

1,043件の閲覧回数
DerekDai
Contributor II

Disable serial console in kernel, remove kernel argument (console=XXX) from kernel command line. If you still need a console, try telnet, ssh through ethernet.

0 件の賞賛
返信