To transition from low power mode to high power mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To transition from low power mode to high power mode

ソリューションへジャンプ
1,455件の閲覧回数
tamotsu
Contributor IV

I debugging IVT of i.MX7D.

The boot device is parallel NOR Flash using EIM interface.

After powerup, the CORE is going to read  the NOR flash.

However, it stop after reading 20 words because there are error in the content.

A message appears in the debugger saying that the 1V power supply is 0V and halt cannot be performed.

How can I set it to high power mode?

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,178件の閲覧回数
tamotsu
Contributor IV

I solved it myself.

After changing the boot-device from NOR-FROM to QSPI, the Boot-ROM dose not enter Low-Power-Mode after booting.

Then connect the debugger and the connection was completed.

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,442件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

What bootloader are you using?

0 件の賞賛
返信
1,439件の閲覧回数
tamotsu
Contributor IV

Hello jimmychan.

This is the state before bootloarder.

When the power is turned on, the built-in ROM gose to read the IVT.

Then the MPU ends up in the state of my question.

Best regards.

0 件の賞賛
返信
1,358件の閲覧回数
tamotsu
Contributor IV

After POR, the boot ROM reads the IVT.

Please tell me what to execution with the boot ROM after an error occurs.

 

0 件の賞賛
返信
1,179件の閲覧回数
tamotsu
Contributor IV

I solved it myself.

After changing the boot-device from NOR-FROM to QSPI, the Boot-ROM dose not enter Low-Power-Mode after booting.

Then connect the debugger and the connection was completed.

 

0 件の賞賛
返信