Timings for Ampire lcd with imx8mp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Timings for Ampire lcd with imx8mp

1,162件の閲覧回数
Destel
Contributor I
 
Hi,

I'm trying to set timings of the lcd AM-19201080D1TZQW-T02H in order to connect display to an embedded board with IMX8MP processor.

I customized device tree node with the following values, read in the display specification:

panel_lvds: panel-lvds {
compatible = "panel-lvds";
 
width-mm = <210>;
height-mm = <158>;
data-mapping = "vesa-24";
status = "okay";
 
panel-timing {
clock-frequency = <70930000>;
hactive = <960>;
vactive = <1080>;
hfront-porch = <430>;
hback-porch = <105>;
vfront-porch = <30>;
vback-porch = <0>;
                        de-active = <1>;
                        hsync-active = <0>;
                        vsync-active = <0>;
};
 
port {
panel_in_lvds: endpoint {
remote-endpoint = <&lvds0_out>;
};
 
&ldb {
status = "okay";
 
        fsl,dual-channel;
lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";
 
port@1 {
reg = <1>;
 
lvds0_out: endpoint {
remote-endpoint = <&panel_in_lvds>;
};
};
};
};
};
};
 
With these configuration display does not work. Sometimes display turn on with only a green backlight.
 

The timing specifications are: 

Destel_1-1693294275464.png

 

What am I doing wrong?
Can you help me?
 
Thanks and regard
0 件の賞賛
返信
2 返答(返信)

1,106件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Destel 

 

1.hactive should be 1920, the other horizontal parameters should be double.

2.You need add new PLL RATE in imx_pll1443x_tbl, PLL VALUE=PIXEL CLOCK *7 (dual channel mode)

drivers/clk/imx/clk-pll14xx.c

 

 

static const struct imx_pll14xx_rate_table imx_pll1443x_tbl[] = {
	PLL_1443X_RATE(1039500000U, 173, 2, 1, 16384),
	PLL_1443X_RATE(650000000U, 325, 3, 2, 0),
	PLL_1443X_RATE(594000000U, 198, 2, 2, 0),
	PLL_1443X_RATE(519750000U, 173, 2, 2, 16384),
	PLL_1443X_RATE(393216000U, 262, 2, 3, 9437),
	PLL_1443X_RATE(361267200U, 361, 3, 3, 17511),
};

 

 

For pkms parameters, you can calculate it from page 265 in RM

 
 
 

 

 

0 件の賞賛
返信

1,077件の閲覧回数
Destel
Contributor I

Hi,

I don't think it's a pll rate problem. I modified timing values  with the following suggested by supplier:

panel-timing {
clock-frequency = <141000000>;
hactive = <1920>;
vactive = <1080>;
hsync-len = <22>;
hfront-porch = <100>;
hback-porch = <100>;
vsync-len = <2>;
vfront-porch = <10>;
vback-porch = <8>;

de-active = <0>;
hsync-active = <0>;
vsync-active = <0>;
pixelclk-active = <0>;
swap-rb = <0>;
swap-rg = <0>;
swap-gb = <0>;
};

Now monitor is working, but flickering problem on monitor still remain. Maybe some settings are wrong?

Can you help me?

 

0 件の賞賛
返信