Thunderbolt compatible with iMX8MPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Thunderbolt compatible with iMX8MPlus

Jump to solution
2,361 Views
GuiDas
Contributor II

Hello,

 

I am currently working on the iMX8MPlus and I would like to know if the USB 3.0 connected to an USB C connector  could be compatible with the Thunderbolt protocol ?

 

Thank you in advance,

 

Guilhem

0 Kudos
Reply
1 Solution
2,356 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello GuiDas,

It could be compatible but the transfer going to be as usb 3.0.

Regards

 

View solution in original post

0 Kudos
Reply
3 Replies
2,357 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello GuiDas,

It could be compatible but the transfer going to be as usb 3.0.

Regards

 

0 Kudos
Reply
2,346 Views
GuiDas
Contributor II

Thank you for you answer, I just need a precision,when you say "transfer going to be as usb 3.0", you mean the data rat ?

I have another question following your answer, do I need to implement something special in hardware/software in order to have the thunderbolt ?

Thank you,

Guilhem

0 Kudos
Reply
2,320 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi, yes i refer to data rate and not change from I.MX side.

regards

 

0 Kudos
Reply