These packages failed to build: minicom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

These packages failed to build: minicom

Jump to solution
962 Views
vishvapathi
Contributor V

Processing: minicom

=====================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try minicom_2.2.orig.tar.gz from the GPP

Read error (Connection timed out) in headers.

Can't get: minicom_2.2.orig.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Wed Jul 17 11:59:59 2013

Ended:   Wed Jul 17 12:00:15 2013

Elapsed: 16 seconds

These packages failed to build:

minicom

Build Failed

Exiting on error or interrupt

Since there versions are updated the older once are not available i guess. How do i up date the ltib to look for the updated version in below link?

http://ftp.debian.org/debian/pool/main/m/minicom/minicom_2.6.2.orig.tar.gz


I have also manually downloaded the same to pkgs folder of LTIB, how do i make the LTIB to check the pkg folder instead of older version online.


Kindly advice

Labels (2)
0 Kudos
Reply
1 Solution
729 Views
4guin4g4
Contributor IV

Modify the Makefile and Kconfig, to have ltib compile the new package.

View solution in original post

0 Kudos
Reply
1 Reply
730 Views
4guin4g4
Contributor IV

Modify the Makefile and Kconfig, to have ltib compile the new package.

0 Kudos
Reply