There is some lib missing when build Firefox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

There is some lib missing when build Firefox

1,370 次查看
wangvictor
Contributor III

Hi All:

I am using Firefox as my browser with x11.

I build firefox with this command `bitbake firefox`.

It all fine during the compiling.

But here is the problem when I execute firefox in my rootfs.

Here is the error that I got:

XPCOMGlueLoad error for file /usr/lib/firefox-38.4/libxul.so:

libvpx.so.2: Cannot open shared object file: No such file or directory

Couldn't load XPCOM.

When I check the library that yocto project built out and found no libvpx.so.2.

How to solve this question?

Thanks in Advanced.

标签 (4)
标记 (3)
0 项奖励
回复
1 回复

1,131 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wang

for firefox one can check boundary devices releases:

Morty Yocto Release i.MX6 Series - NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复