The watchdog timeout fails to restart the Linux system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The watchdog timeout fails to restart the Linux system

3,741件の閲覧回数
lixoyv
Contributor II

The NXP IMX6Q chip is used, and the Linux system is Ubuntu16.0.4. The system is mounted with a pcie device, and the watchdog times out to restart the Linux system. There is a problem during the restart process, and it stops at "1ffc000.pcie supply pcie-bus not found, using dummy regulator", not sure if it stopped because of this message. However, rebooting the system can be done using the reboot command or by pressing the reset key on the device. See the attachment for the messages of the three restart methods.

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

3,737件の閲覧回数
Yuri
NXP Employee
NXP Employee

@lixoyv 
Hello,

   It is highly recommended to remove power from all board
components in case of processor reset in order to avoid issues
with undefined state of components critical for reboot.
 

  So, total system POR may be recommended for reboot (via WDOG).
Please verify Your design if this is so. Use the reference design as
an example.

Regards,
Yuri.

0 件の賞賛
返信

3,730件の閲覧回数
lixoyv
Contributor II

The watchdog only resets the cpu. Is there a way to solve this problem without changing the hardware design?

3,726件の閲覧回数
Yuri
NXP Employee
NXP Employee

@lixoyv 

If only CPU is reset - the results may be un-predictable.

 

~Yuri.

0 件の賞賛
返信

3,723件の閲覧回数
lixoyv
Contributor II

Can you guys test it and give a definite answer。

0 件の賞賛
返信