The watchdog timeout fails to restart the Linux system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The watchdog timeout fails to restart the Linux system

3,520 次查看
lixoyv
Contributor II

The NXP IMX6Q chip is used, and the Linux system is Ubuntu16.0.4. The system is mounted with a pcie device, and the watchdog times out to restart the Linux system. There is a problem during the restart process, and it stops at "1ffc000.pcie supply pcie-bus not found, using dummy regulator", not sure if it stopped because of this message. However, rebooting the system can be done using the reboot command or by pressing the reset key on the device. See the attachment for the messages of the three restart methods.

标签 (3)
0 项奖励
回复
4 回复数

3,516 次查看
Yuri
NXP Employee
NXP Employee

@lixoyv 
Hello,

   It is highly recommended to remove power from all board
components in case of processor reset in order to avoid issues
with undefined state of components critical for reboot.
 

  So, total system POR may be recommended for reboot (via WDOG).
Please verify Your design if this is so. Use the reference design as
an example.

Regards,
Yuri.

0 项奖励
回复

3,509 次查看
lixoyv
Contributor II

The watchdog only resets the cpu. Is there a way to solve this problem without changing the hardware design?

3,505 次查看
Yuri
NXP Employee
NXP Employee

@lixoyv 

If only CPU is reset - the results may be un-predictable.

 

~Yuri.

0 项奖励
回复

3,502 次查看
lixoyv
Contributor II

Can you guys test it and give a definite answer。

0 项奖励
回复