The system locks when enable CSI data transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The system locks when enable CSI data transfer

1,512件の閲覧回数
zhenboliu
Contributor I

#

Hello, I am from Aratek Shenzhen, now we are using IMXU6L CSI interface to collect image data, we encountered a problem that when enable CSI data transfer,the system will be locked up soon.  could you give us some suggestions to fix this issue.

thanks!

Darren 

[email protected]

#

ラベル(1)
0 件の賞賛
返信
1 返信

1,452件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhenbo

one can check hardware, clocks and power using

Hardware Development Guide for the i.MX 6UltraLite Applications Processor
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf

and run memory test

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信