The system locks when enable CSI data transfer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The system locks when enable CSI data transfer

1,507 Views
zhenboliu
Contributor I

#

Hello, I am from Aratek Shenzhen, now we are using IMXU6L CSI interface to collect image data, we encountered a problem that when enable CSI data transfer,the system will be locked up soon.  could you give us some suggestions to fix this issue.

thanks!

Darren 

[email protected]

#

Labels (1)
0 Kudos
Reply
1 Reply

1,447 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhenbo

one can check hardware, clocks and power using

Hardware Development Guide for the i.MX 6UltraLite Applications Processor
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf

and run memory test

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply