The mipi output problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The mipi output problem

3,077件の閲覧回数
pingyuchen
Contributor II

Hi,

Now  I use the imx8mq evk board to test the mipi output. I use boot-imx8mq-mipi-panel.img and can measure the mipi signal when the board is booted. But I find the mipi signal isn't output when the board is resumed from the suspend mode by ON/OFF button. Where can I modify to fix this problem?

Best Regards,

0 件の賞賛
返信
4 返答(返信)

2,918件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi pingyu

this issue is described in Table 13. Known issues and workarounds for i.MX 8MQuad

attached Release Notes.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,918件の閲覧回数
pingyuchen
Contributor II

Hi Igor,

Thank you for your response. By the way, is there a scheduler for the new release? And can this issue be solved in the new release if we need the system suspending and resuming?

0 件の賞賛
返信

2,918件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi pingyu

one can try attached patch and Linux L4.9.123

linux-imx - i.MX Linux kernel 

Best regards
igor

0 件の賞賛
返信

2,917件の閲覧回数
pingyuchen
Contributor II

Hi igor,

I used the patch and this issue is fixed.

Thank you very much!

0 件の賞賛
返信