The method about RTC test on MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The method about RTC test on MX6DL

1,814 Views
tony_l_cai
Contributor III

Hi,all

     could you give me a method about internel RTC module test on MX6DL? Our customized board need a method(it means a interface via userspace) to test the RTC module whether it works well. For example, can I read some values from some registers ,which makes me judging the work status about the RTC module ?  

Can you give me a help? 3Q~

Labels (2)
0 Kudos
Reply
3 Replies

1,734 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

one can look at imx-test package included in ltib, it has many tests

for processor modules

..imx-test-3.0.35-4.1.0/test/mxc_rtc

L3.0.35_4.1.0_DEMO_IMAGE_BSP

L3.0.35_4.1.0_ER_SOURCE_BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,734 Views
tony_l_cai
Contributor III

Dear igor,

     maybe I just want a register or or interface to know the RTC is not wrong, and it can work well, could I have?

0 Kudos
Reply

1,734 Views
igorpadykov
NXP Employee
NXP Employee

more simple way with SDK rtc test:

i.MX 6Series Platform SDK

0 Kudos
Reply