The i.RAM(OCRAM) effective use way

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The i.RAM(OCRAM) effective use way

ソリューションへジャンプ
3,756件の閲覧回数
george
Senior Contributor II

Dear all,

I develops the product which used i.MX6.

I want to use original RTOS, without using linux.

And I use iRAM (OCRAM) for operation speed-up.

Please tell me the way for speed-up of iRAM and CPU-core.

a)  Please tell me the iRAM clock speed change method.

b)  Please let me know the care point.

c)  Is there any idea for speed-up?

d)  Is there any document relevant to them?

Best Regards,

George

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,316件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, George

     I looked into the CCM of i.MX6Q, the OCRAM's clock parent is AHB, and AHB is 133MHz when kernel boot up and AHB is system's clock, its max freq is 133MHz according to RM table 18-3. So as far as I know, we should NOT increase OCRAM's clk freq. But I do see there is write/read pipeline function in OCRAM chapter which might impact the delay of data read/write, it is controlled by IOMUX_GPR3[24:21], you can look through the RM chapter of OCRAM and IOMUX_GPR for details.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,316件の閲覧回数
bk300
Contributor I

I was curious if there was any further information on the OCRAM's speed?

I'm currently using an iMX6Q and am attempting to use the OCRAM as a shared memory between threads.  I wrote a quick test that looks similar to the following psuedo code...

Set GPIO pin HIGH

// Loop 1 million times

for( x = 0; x < 1000000; x++ )

{

     *(0x00900000) = x;  // Write to OCRAM

    y = *(0x00900000);   // Read from OCRAM

}

Set GPIO pin LOW

I monitored the GPIO pin using an oscope and the delay measured to be about 1 second.  At 1 million loops, the delay for a read/write pair to the OCRAM is about 1 microsecond...which seems really slow.  I've already disabled the read/write delays by clearing the IOMUX_GPR3[24:21] bits, so I'm not sure what else I can do.  Does anybody have some sort of explanation why the OCRAM appears to be so slow?

Thanks

0 件の賞賛
返信
3,316件の閲覧回数
Yuri
NXP Employee
NXP Employee

Was instruction cache enabled ?

0 件の賞賛
返信
3,317件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, George

     I looked into the CCM of i.MX6Q, the OCRAM's clock parent is AHB, and AHB is 133MHz when kernel boot up and AHB is system's clock, its max freq is 133MHz according to RM table 18-3. So as far as I know, we should NOT increase OCRAM's clk freq. But I do see there is write/read pipeline function in OCRAM chapter which might impact the delay of data read/write, it is controlled by IOMUX_GPR3[24:21], you can look through the RM chapter of OCRAM and IOMUX_GPR for details.

0 件の賞賛
返信
3,316件の閲覧回数
george
Senior Contributor II

Dear Yongcai,

Thank you for the reply.

Helpful very much.

BR,

George

0 件の賞賛
返信