U-BOOT 3.10.17beta nand write support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-BOOT 3.10.17beta nand write support

1,314 Views
xiongweihuang
Contributor III

Hi all

I check out code from http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/log/?h=imx_v2013.04_3.10.17_1.0.0_beta

and on my custom board ,I can read from nand ,

While I try to erase , it get failed .

U-Boot > saveenv

Saving Environment to NAND...

Erasing Nand...

nand0: MTD Erase failure: -5

Writing to Nand... FAILED!

U-Boot > version

U-Boot 2013.04-gc207317-dirty (Mar 04 2014 - 16:50:35)

arm-linux-gnueabihf-gcc (crosstool-NG linaro-1.13.1-4.8-2013.11 - Linaro GCC 2013.10) 4.8.3 20131111 (prerelease)

GNU ld (crosstool-NG linaro-1.13.1-4.8-2013.11 - Linaro GCC 2013.10) 2.23.2.20130610 Linaro 2013.10-4

I dont know if freescale will update about this or ,  is there  anything I missed ?

Thanks and regards

Labels (1)
0 Kudos
Reply
1 Reply

1,089 Views
YixingKong
Senior Contributor IV

Weihuang

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply