The download link of Linux 5.4.3 demo image is error in imx8mq evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The download link of Linux 5.4.3 demo image is error in imx8mq evk board

1,101 Views
hongxingyu1982
Contributor III

I download the 5.4.3 linux version with imx8mq board "LF_v5.4.y-1.0.0_images_MX8MQEVK.zip"in the blew link :

Linux L4.14.98_2.0.0_GA; SDK2.5.2_8QXP/8QM_PostGA, SDK2.5.1_7ULP_GA3 Release Announcement 

But when I used the uuu tools flash it to emmc, It says error as blew:

pastedImage_2.png

Is there any way to download linux 5.4.3 demo image for i.mx8mqEVK?

 

Thanks~

 

BR,

0 Kudos
Reply
1 Reply

1,077 Views
joanxie
NXP TechSupport
NXP TechSupport

the link you sent is for 4.14.98, for 5.4.3, you can download from the link as below:

Embedded Linux for i.MX Applications Processors | NXP ”

focus on the "L5.4.3_1.0.0_MX8MQ"

0 Kudos
Reply