The dev_no between uboot and kernel blk device.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The dev_no between uboot and kernel blk device.

1,228件の閲覧回数
wenmingfeng
Contributor III

Hello,

imx6 chip expertise,

I have an imx6dl customer board refer from imx6dlsabresd, the MMC i used is connect to MX6_PAD_SD1, and in uboot I set the dev_no=0 so it can find the mmc 0, what is the correct parameter transfer to kernel, => printenv mmcdev
mmcdev=0
=> printenv mmcroot
mmcroot=/dev/mmcblk0p2 rootwait rw
If this is wrong, then what is the correctly mapping? 

ラベル(2)
0 件の賞賛
返信
1 返信

1,153件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About the parameter settting in u-boot you can refer to the documents i.MX_Linux_Release_Notes.pdf and i.MX_Linux_User's_Guide.pdf. section 4 Kernel Boot Parameters and 4.7.1 Running Linux OS from MMC/SD.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信