The access method to PCIE_RC_BAR0 register.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The access method to PCIE_RC_BAR0 register.

ソリューションへジャンプ
1,983件の閲覧回数
george
Senior Contributor II

Dear All,

We have planned the product which used i.MX6DL.

And, The product works PCIe on RTOS.

We are investigating how to use PCIe and are investigating the access method to PCI-Configuration space now.

In " i. MX 6Solo/6 DualLite Applications Processor Reference Manual, Rev.1, and 04/2013 ",

PCIE_RC_BAR0 register modification is described to be "Bits[3:0] are writable through the DBI."

Please tell me the PCIE_RC_BAR0 register modification method via DBI.

* I cannot find the materials about it.

Best Regards,

George

ラベル(6)
0 件の賞賛
返信
1 解決策
1,777件の閲覧回数
b47504
NXP Employee
NXP Employee

In RC side, you should be able to modify the register directly. As you know, for CDM space,  you can modify some of them through local bus, or by the remote partner through pcie wire. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,778件の閲覧回数
b47504
NXP Employee
NXP Employee

In RC side, you should be able to modify the register directly. As you know, for CDM space,  you can modify some of them through local bus, or by the remote partner through pcie wire. 

0 件の賞賛
返信
1,777件の閲覧回数
george
Senior Contributor II

Dear Yuan,

Thanks.

0 件の賞賛
返信