The Camera Image is Split.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Camera Image is Split.

Jump to solution
3,115 Views
donggyulee
Contributor I

Hi All,

I'm testing the camera of i.mx6 demo kit.

(The Board is SabreSD 6Q)

The camera image is not good.

The Camera image was split in two.

Please Check the attached file.

My System :

     Linux 3.0.101

     Camera Module : OV5640 Mipi

     Test command :  ./unit_tests/mxc_v4l2_overlay.out -iw 1920 -ih 1080 -ow 1920 -oh 1080 -di /dev/video1

Please advise.

Thank you

0 Kudos
Reply
1 Solution
2,944 Views
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

seems driver does not cover the 1080p 30fps option and although it’s theoretically possible

to achieve, it would require the coefficient  pair values to tweak the frame rate. These coefficient

tables are given by Omnivision. One can use drivers provided for other boards, like Sabre Lite board.

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.10.17_1.0.0_ga/drivers/media/platf...

Alternatively one may look for other 3rd party efforts:

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,945 Views
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

seems driver does not cover the 1080p 30fps option and although it’s theoretically possible

to achieve, it would require the coefficient  pair values to tweak the frame rate. These coefficient

tables are given by Omnivision. One can use drivers provided for other boards, like Sabre Lite board.

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.10.17_1.0.0_ga/drivers/media/platf...

Alternatively one may look for other 3rd party efforts:

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,944 Views
donggyulee
Contributor I

Hi igor

Thank you so much

You are a nice guy:smileyhappy:

0 Kudos
Reply