Text/Image overlay on VPU data using IPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Text/Image overlay on VPU data using IPU

2,808 Views
subodh
Contributor III

Hi,

I want to overlay text on the data returned by VPU.

When I play AVC data the mxc_vpu_test.out always outputs NV12.

Also when I use the above test case with IPU_PATH, I do not see any video on screen.

It works only with V4L2.

DirectFB cannot perform overlay unless this video is rendered as ARGB.

Reference for failed color space conversion.

https://community.freescale.com/thread/328328

Please suggest a solution to get overlays working on IMX6Q using DirectFB or any other API providing direct text overlay API.

Labels (4)
0 Kudos
Reply
2 Replies

2,104 Views
jamesbone
NXP TechSupport
NXP TechSupport

So far,  I understand that only V4L2 it is the only implemented  sink that we have in the i.MX6 BSP .  are you using Gstreamer? or what are you using or want to use to play the video.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,104 Views
subodh
Contributor III

As of now I am not using gstreamer, just working with VPU API test case modified for my experiments.

But I want to explore all available options before I can pick one.

Please suggest if gstreamer-imx plugins are stable and complete enough for such operations. If not what are

other options available for me.

Thanks

Regards,

Subodh

0 Kudos
Reply