Testing signed images

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Testing signed images

Jump to solution
3,672 Views
eduardo3
Contributor III

Hello,

I am in the process of adding signed images to our board but I was left with questions on how to test that.

After getting a signed os_cntr_signed.bin image, it boots fine. On u-boot when I try ahab_status, I see SECO events (because I don't have my keys fused yet).

Initially I thought I could use u-boot fuse override for testing the fuse values I need to use, but that is not implemented. After searching on how to use fuse shadow registers, I found that it is not possible. Examples:

https://community.nxp.com/t5/i-MX-Processors/Access-to-OCOTP-registers-from-SCU-on-IMX8QM-leads-to-h...

https://community.nxp.com/t5/i-MX-Processors/IMX8-unable-to-override-OCOTP-shadow-registers-Is-there...

Initially If thought I could implement something like what is mentioned in the first link.

Based on that, how am I supposed to test secure boot keys / commands without permanently fusing the keys or bricking the board?

What is NXP advice on that?

For reference, we are using i.MX8X (imx8qxp).

 

0 Kudos
Reply
1 Solution
3,625 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If not burning the SRK fuse, you may can use OPENSSL command to analyze the images with their key.

 

Regards

View solution in original post

0 Kudos
Reply
3 Replies
3,596 Views
eduardo3
Contributor III

I'll try the openssl approach in the future. Another FAE we contacted also confirmed there is no way of testing on a imx8 board without fusing the keys. His suggestion in that case was to fuse (if we are fine with that) but not close the device.

0 Kudos
Reply
3,626 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If not burning the SRK fuse, you may can use OPENSSL command to analyze the images with their key.

 

Regards

0 Kudos
Reply
2,004 Views
imx8mp_developer
Contributor I

I am interested in this topic!
I need to verify the os_cntr_signed.bin container coming out from a Yocto AHAB-signed build for imx93

If I do:
~/cst-4.0.0/linux64/bin/ahab_image_verifier os_cntr_signed.bin 0 0


I get:

Signature Block:
 Version: 0
 Length: 2648 bytes
 Tag: 0x90
 Certificate Offset: 0x0
 SRK Table/Array Offset: 0x10
 SRK Table:
   Tag: 0xD7
   Length: 2112 bytes
   Version: 66
   SRK Record:
     Tag: 0xE1
     Length: 527 bytes
     Sign Algorithm: RSA       
     Hash Algorithm: SHA2_384       
     Key Size/Curve: RSA4096       
     SRK Flags: CA Flags       
     Modulus (N):
.....
Signature verification failed

This doesn't happen for imx-boot-imx93-var-som-aski-sd.bin-flash_singleboot_gdet

Signature Block:
 Version: 0
 Length: 400 bytes
 Tag: 0x90
 Certificate Offset: 0x0
 SRK Table/Array Offset: 0x10
 SRK Table:
   Tag: 0xD7
   Length: 308 bytes
   Version: 66
   SRK Record:
     Tag: 0xE1
     Length: 76 bytes
     Sign Algorithm: ECDSA       
     Hash Algorithm: SHA2_256       
     Key Size/Curve: PRIME256V1       
     SRK Flags: None       
     X Coordinate:  ....
     Y Coordinate:  ...

......

Signature verification successful

I am using a Digicert HSM for the signature

does anybody have a clue about the verification failed for os_cntr_signed ?
does anybody have a hint on how to verify the signature with openssl ?(just to exclude the issue is ahab_image_verifier itself)

0 Kudos
Reply