Testing LPDDR4 in imx9 series board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Testing LPDDR4 in imx9 series board

2,741 Views
Robbi
Contributor II

HI team, 

                I had a Custom board with imx-9 processor and LPDDR4 RAM. I need to test the entire 8GB ram memory, kindly help with reference or links to test.

Tags (1)
0 Kudos
Reply
5 Replies

2,716 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

i.MX93 supports up to 2GB DDR memory space.

To test DDR memory in i.MX devices, I suggest you use Config Tools for i.MX.

Best regards.

0 Kudos
Reply

2,665 Views
Robbi
Contributor II

Hi @JorgeCas ,

    Thanks for reply. As per instruction, installed imx config tool. Please check Image attached below, is this the correct approach to check LPDDR4. And can you provide me any user manual.

 

 

Thanks, and regards,

Robbi 

 

 

0 Kudos
Reply

2,647 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Please take a look in the next link.

Best regards.

2,342 Views
Robbi
Contributor II
Hi @jorge,
Thanks for the reply, can I use memtester also to test LPDDR. And I installed MCUXpressoIDE try to download SDK for imx93 unable to install. Can you help me on it.
0 Kudos
Reply

2,027 Views
Robbi
Contributor II

Hi @JorgeCas ,

                 Thanks for support.  Does i.MX config tool supports imx7D and imx8 processors. Because, I had custom board with MCIMX7D5EVK10SD where I'm unable to enable DDR tool for validation.

Robbi_0-1735020048949.png

 

Please check the attached image for reference.

Thanks

Robbi

Tags (1)
0 Kudos
Reply