Tamper detection implementation in i.MX8X processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Tamper detection implementation in i.MX8X processor

跳至解决方案
2,641 次查看
puneethkumar
Contributor III

Dear Team,

I am planning to implement a tamper detection in my system.

Can anyone send reference where we can understand what is the difference between active & passive tamper detection.

I have planned to use only two tamper pins for the detection.

SNVS_Tamper_In & SNVS_Tamper_Out.

I will use a 3 pin header - through my enclosure i will short the Tamper in & Tamper out pins, if anyone removes the enclosure that time the connection between tamper in & tamper out pins will be removed, so that we can identify if tamper is happened.

Please let me know whether the implementation method is proper or not

0 项奖励
回复
1 解答
2,637 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复
1 回复
2,638 次查看
igorpadykov
NXP Employee
NXP Employee

Hi puneethkumar

 

this information can be found in

Security Reference Manual for i.MX8DualX/8DualXPlus/8QuadXPlus Application Processors

 

Best regards
igor

0 项奖励
回复