Taking Qt application Remote running on i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Taking Qt application Remote running on i.MX6UL

1,188 Views
Poornesh7
Contributor II

I am using i.MX6UL SoC with my custom hardware . I have built yocto with "DISTRO : fsl-imx-fb" , now I am running my QT application with 7 inch touch screen LCD interfaced to it.

Now it is required to take my QT application remotely and interacted from my remote client. Kindly requesting you for the suggestions on what packages need to add in my yocto to achieve this.

Yocto version : Yocto Zeus. I dont want to use x11.

Labels (1)
0 Kudos
Reply
3 Replies

1,112 Views
Poornesh7
Contributor II

@jimmychan, thanks for the reply .


As mentioned above ,  I am using Yocto version - 3.0 (zeus) , kernel version - 5.4-r0 .

Now my requirement is to take my QT application remotely and interacted from my remote client . For this I need your suggestions/procedure on what packages need to add in my yocto to achieve this.

I dont want to use x11..

 

Thanks

0 Kudos
Reply

1,104 Views
jimmychan
NXP TechSupport
NXP TechSupport

We have different version of BSP that the kernel is L5.4.xx. Please select one of them to use and build.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

>> "QT application remotely and interacted from my remote client . ". 

 

We don't have similar QT example. For the QT application example, I would suggest you to consult the QT forum or find the example in Google. 

 

e.g. https://community.teamviewer.com/English/kb/articles/109833-grab-remote-screen-for-qt-applications

 

 

0 Kudos
Reply

1,168 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

What is the issue? Could you tell me more details? any error message?

0 Kudos
Reply