TW9912

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
10,714 次查看
强王
Contributor IV

TW9912驱动

附件是驱动和dts配置

 

注意事项:

1:信号源

CVBS_IN >> YIN1

 

对应寄存器0x02 – Input Format (INFORM)

 

 

2:i2c地址

 

If the SIAD pin is tied to VDD33, then the least significant bit of the 7-bit address is a “1”. If the SIAD pin is tied to VSS33 then the least significant bit of the 7-bit address is a “0”.

如果接地SIAD是1,接电是0

我们原理图是0x45

Original Attachment has been moved to: dts.zip

Original Attachment has been moved to: tw9912.c.zip

标记 (1)
1 解答
9,347 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

for TW9912 usage with i.MX6S one can look at

Switching CSI into Progressive bt.656 Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

6 回复数
9,347 次查看
强王
Contributor IV

我已经调好了,有需要的朋友可以给我留言

0 项奖励
回复
9,347 次查看
lvguangzhao
Contributor I

需要tw9912的驅動, 能否分享呢?

感謝.

0 项奖励
回复
9,347 次查看
强王
Contributor IV

已上传

0 项奖励
回复
9,347 次查看
xiaochaoxu
Contributor I

您好,我目前也在调试TW9912,出现画面切割问题,能否提供下TW9912驱动,给我参考下,谢谢。

0 项奖励
回复
9,347 次查看
542168009
Contributor I

您好,您的TW9912是否已经调好,有几点疑问,能否解答一下啊,万分感激!

0 项奖励
回复
9,348 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

for TW9912 usage with i.MX6S one can look at

Switching CSI into Progressive bt.656 Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------