TW9912

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
10,695件の閲覧回数
强王
Contributor IV

TW9912驱动

附件是驱动和dts配置

 

注意事项:

1:信号源

CVBS_IN >> YIN1

 

对应寄存器0x02 – Input Format (INFORM)

 

 

2:i2c地址

 

If the SIAD pin is tied to VDD33, then the least significant bit of the 7-bit address is a “1”. If the SIAD pin is tied to VSS33 then the least significant bit of the 7-bit address is a “0”.

如果接地SIAD是1,接电是0

我们原理图是0x45

Original Attachment has been moved to: dts.zip

Original Attachment has been moved to: tw9912.c.zip

ラベル(5)
タグ(1)
1 解決策
9,328件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

for TW9912 usage with i.MX6S one can look at

Switching CSI into Progressive bt.656 Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

6 返答(返信)
9,328件の閲覧回数
强王
Contributor IV

我已经调好了,有需要的朋友可以给我留言

0 件の賞賛
返信
9,328件の閲覧回数
lvguangzhao
Contributor I

需要tw9912的驅動, 能否分享呢?

感謝.

0 件の賞賛
返信
9,328件の閲覧回数
强王
Contributor IV

已上传

0 件の賞賛
返信
9,328件の閲覧回数
xiaochaoxu
Contributor I

您好,我目前也在调试TW9912,出现画面切割问题,能否提供下TW9912驱动,给我参考下,谢谢。

0 件の賞賛
返信
9,328件の閲覧回数
542168009
Contributor I

您好,您的TW9912是否已经调好,有几点疑问,能否解答一下啊,万分感激!

0 件の賞賛
返信
9,329件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

for TW9912 usage with i.MX6S one can look at

Switching CSI into Progressive bt.656 Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------