TW9910 Video Capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TW9910 Video Capture

2,079件の閲覧回数
andrekilian
Contributor I

Hi,

I am trying to capture a Video from a TW9910 on our IMX6Q (We run Android 5.0.2 with 3.10.53 Kernel)

Analog Camera ---->TW9910 -----BT656----> imx6q CSI0

I took the ADV7180 driver from  "/drivers/media/platform/mxc/capture/adv7180" and removed all the I2C communication related to ADV7180.Then I used the following code to initialize the TW9910 for ITU-R BT.656 (according to the datasheet):

    i2c_smbus_write_byte_data(priv->client,0x02, 0x40);
    i2c_smbus_write_byte_data(priv->client,0x03, 0xA6);

   

   //######## BT.656 (Datasheet)

    i2c_smbus_write_byte_data(priv->client,VDELAY_LO,     0x012); //VDELAY_LO
    i2c_smbus_write_byte_data(priv->client,VACTIVE_LO,     0x0F4); //VACTIVE_LO
    i2c_smbus_write_byte_data(priv->client,HACTIVE_LO,     0x2D0); //HACTIVE_LO

    i2c_smbus_write_byte_data(priv->client,VBICNTL,     0x58); //HA_EN 1
    i2c_smbus_write_byte_data(priv->client,DID,         0x20); //VIPCFG 1
    i2c_smbus_write_byte_data(priv->client,VVBI,         0x10); //NTSC656 1

To test it I tried to capture a Video with

cat /dev/video0 > /sdcard/test1.mpeg

however the IPU seems to lose the incoming frames:

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
.

.

.

Capturing with ffmpeg:

ffmpeg-2.2.git -f v4l2 -framerate 30 -video_size 640x480 -pix_fmt uyvy422 -i /dev/video0 /sdcard/output.mkv

TW9910capture1.png

I also tried to use gstreamer-imx from GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms 

but was unable to install it.

What could be the problem with the IPU losing Frames? Do I need another configuration for TW9910, or other tools to test it?

0 件の賞賛
返信
1 返信

1,718件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andre

please check

Switching CSI into Progressive bt.656 Mode 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信