TVE - S-Video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TVE - S-Video

1,913件の閲覧回数
G1z
Contributor I

I'm working on a design using the i.MX535 and would like to use the TV Encoder outputs as S-Video. Reading thru the documentation it is not clear to me which TVDAC outputs should be used. The datasheet pinouts only indicate TVDAC_IOR, IOG, and IOB for VGA mode.

In which document can I find the pinouts for S-Video Chroma and Luma outputs?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,824件の閲覧回数
G1z
Contributor I

Thanks Nitin.

If I understand the table correctly, shown below, the pin labeled TVDAC_IOR would be Chroma (C) and TVDAC_IOG would be Luma (Y)? TVDAC_IOB is unused or could be composite video.

0 件の賞賛
返信

1,824件の閲覧回数
NitinSonar
Contributor I

Hi,

For TVOUT, there is no extra circuitry required. Refer to Tale No 73-3 TVE output data.

You need to change the only operating mode and you can use the single channel of VGA connector as reference circuit 75ohm driving capability. There may be additional passive circuit may be needed to match 75E impedance.

Best Regards

Nitin Sonar

 https://community.nxp.com/discussions/104-TVOUT.png" target="_self

0 件の賞賛
返信