TUN/TAP interface in im6ul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TUN/TAP interface in im6ul

2,268 次查看
vijayaragavansr
Contributor II

Hi Folks,

how to enable the tun/tap device in im6ul? if it in the kernel how to do that?

which kernel config will enable the tun/tap device?

Thanks

Vijay

0 项奖励
回复
2 回复数

2,028 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vijayaragavan

I am afraid this is not supported in nxp bsps, however one can add

it using generic linux driver examples:

http://stackoverflow.com/questions/1003684/how-to-interface-with-the-linux-tun-driver
http://vtun.sourceforge.net/tun/faq.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,028 次查看
vijayaragavansr
Contributor II

Hi,

Thank. i shall try this out.

Thanks

Vijay

0 项奖励
回复